udpAddrMake
Function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Build an address buffer for UDP User Datagram Protocol functions.
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
En |
BOOL |
0, 1 |
N/A |
No default |
Execute the function. |
IPaddr |
STRING |
0.0.0.0, 255.255.255.255 |
N/A |
No default |
IP address in the form |
port |
DINT |
0, 65535 |
N/A |
No default |
IP port number. |
add[ ] |
USINT |
0, 32 |
N/A |
No default |
Buffer containing the UDP address (filled on output). |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
OK |
BOOL |
|
N/A |
Returns TRUE when the function successfully executes. |
Remarks
- This function:
- Builds an address buffer for UDP functions.
- Is required for building an internal UDP address to be passed to the udpSendTo function in case of UDP client processing.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
bAddrMake := udpAddrMake('10.156.238.176',Server_Port,add); //server details