udpClose
Function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Closes a socket.
Inputs
Input |
Data Type |
Range |
Unit |
Default |
Description |
---|---|---|---|---|---|
En |
BOOL |
0, 1 |
N/A |
No default |
Execute the function. |
sock |
DINT |
0, 65535 |
N/A |
No default |
IP of the socket. |
Outputs
Output |
Data Type |
Range |
Unit |
Description |
---|---|---|---|---|
OK |
BOOL |
|
N/A |
Returns TRUE when the function successfully executes. |
Remarks
None
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
udpClose(Socket_Number); //Close socket