Overview: Create and/or Call Functions & Function Blocks
To call a function A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. or function block A function block groups an algorithm and a set of private data. It has inputs and outputs.:
- Drag an item from the Libraries into a program The act of performing a sequence of instructions or commands.
- Name the new instance of the function or function block
See Call Functions or Function Blocks for more in-depth information.
To create a function or function block:
- Declare the function or function block by right-clicking on Subprograms in the Project Tree.
- Name the function or function block
- Define the inputs and outputs, and any private variables
- Call the new function or function block
See Create Functions and Function Blocks for more in-depth information.