ENI File tab
During the compilation, the KAS-IDE Kollmorgen Automation Suite - Integrated Development Environment generates the EtherCAT Ethernet ofr Control Automation Technology. EtherCAT® is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT is to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs. Network Information (ENI) file based on the EtherCAT devices defined in the project.
Figure 1: ENI File tab
Import or Export an EtherCAT ENI File
Item |
Description |
Used to browse and select an ENI file to be imported.
|
|
Use imported ENI file |
Used to specify whether or not to use the imported ENI file. |
Used to export the ENI file generated by the KAS-IDE Integrated Development Environment - An type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger..
|
-
-
Importing an external ENI file overrides all EtherCAT project device information and configuration settings in the KAS-IDE.
These views and configurations are not applicable when using an imported ENI file:
- Project View: All devices located under the EtherCAT node.
- EtherCAT Device View tabs:
- General Properties
- PDO Process Data Opjects - A type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Selection/Mapping
- Distributed Clock Clock signal.
- CoE Init-Commands
- Slice I/O Properties
- Mapping PLC Programmable Logic Controller - A digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines. Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events. Variables to Slice I/O or PDO objects.
Information displayed in the views may not match the imported ENI file.
Use an Imported ENI File
- The KAS-IDE works in a degraded mode when using an imported ENI file, and the Mapped to Axis settings are disabled Removal of the ENABLE signal.
Disables power stage..
- This is because the information about the devices in the project tree and the EtherCAT widget table is no longer relevant.
- When using an imported configuration file these parameters must be manually set for each axis:
- the type of motion bus.
- its address on the fieldbus An industrial network system for real-time distributed control (e.g., CAN or PROFIBUS, Sercos®).
It is a way of connecting instruments in a plant design. ring.
This is done by right-clicking on the Axis Pipe Block and selecting the Properties command.
- Scan Devices must be run from the EtherCAT Devices tab before downloading the application to the controller.