Log Messages tabs
-
-
Log messages are an important source of information when troubleshooting with KAS-IDE Kollmorgen Automation Suite - Integrated Development Environment.
When reporting an issue to Kollmorgen Support, copy/paste the logs in your report.
Figure 1: Log Messages - Local Log
Log messages are displayed on two tabs, Local log and Controller log.
- The Local Log tab shows all messages managed by the KAS Kollmorgen Automation Suite-IDE Integrated Development Environment - An type of computer software that assists computer programmers in developing software.
IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger. to explain the current state of the system and to help identify any operation errors encountered when developing your system.
- The Controller Log shows all messages managed by the KAS Runtime In computer science, runtime (or run-time) describes the operation of a computer program, the duration of its execution, from beginning to termination (compare compile time). In KAS, runtime refers to the virtual machine that manage the program written in a computer language while it is running..
Based on the configuration settings
-
-
The Configuration button is only available on the Controller log tab when the IDE is connected to a controller.
Every log message in the table widget
Field |
Description |
Time |
Time when the log was recorded with the format:
|
Identifies a software or hardware component issuing the messages. Each source is configured with a specific Level.
|
|
Each message has one of the following levels with importance in ascending order:
|
|
Message |
Text of the message issued from the source
|
Table 3-1: Log Messages - List of Fields
The table contains a contextual menu
Command |
Description |
Disable Removal of the ENABLE signal.
Disables power stage./ |
You can stop the log recording at any time, so that no more messages are added
|
Clear |
Empty the list by erasing all the messages already recorded
|
Copy |
Copy the text of the selected messages to the clipboard (you can perform multi-selection with the Ctrl or Shift keys)
|
Save As |
Save all the messages in a log file
|
Select All |
Select all the messages that are displayed in the table
|
Table 3-2: Log Messages - List of Buttons