Variables tab
Figure 1: Variables tab
The list of variables is split into two parts:
Item Number |
Description |
---|---|
|
All the Variables at the top. |
|
All the Structures at the bottom. |
-
-
See Call Functions or Function Blocks about the procedure to create an instance of a structure.
-
-
To show all the variables of all programs The act of performing a sequence of instructions or commands., select 'PLC Programmable Logic Controller - A digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines. Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events.' in the project tree.
Right-click in the Dictionary window to open the menu:
This menu is used to perform these actions:
Command |
Description |
---|---|
Undo |
Undo the last action performed on the Dictionary. |
Redo |
Redo the last undone action. |
Add Variable |
Add a new variable in the selected level (e.g., Global, Retain, program).
|
Rename variables |
Used to either replace a section of matching variables or append text to the variable's names. See Rename Variables. |
Edit variables as text |
Opens a text editing dialog used to edit the variables found in the group as text using IEC International Electrotechnical Commission - A not-for-profit, non-governmental international standards organization that prepares and publishes International Standards for all electrical, electronic and related technologies. 61131-3 syntax. |
Copy variable value to init value |
Copies the current value of a retain variable to the variable's initial value. |
Browse variable |
Used to browse all instances of a variable. See Browse Variable tab. |
Add Structure |
Used to add a new complex type. A structure named NewStructure is created and variables can be dragged into it. See Complex Structures. |
Rename Structure |
Used to rename the selected structure. |
Copy |
Used to copy a variable. |
Paste |
Used to paste the copied variable to the selected level. |
Delete |
Used to delete the selected variable. Press <Delete> on the keyboard. |
Find all |
Used to find all instances of the specified variable and opens the results in the Find and Replace tab. |
Open UDFB |
Used to open the selected UDFB instance. See Monitoring UDFBs. |
Map to Oscilloscope channel ... |
Used to plug the selected variable on a channel.
|
Unmap all Oscilloscope Channels |
Used to unplug all plugged probes See Softscope - Probe item. from the Softscope. |
Variable I/O mapping |
Used to connect a variable to an I/O. |
Print Dictionary ... |
Used to print all the variables displayed in the Dictionary and sorted by programs. The columns show the Name, Type, Dimension, Initial Value, and Attributes. |
The Track Characterized by an axis group that follows with its movement the movement of another axis group. Selection filters the displayed items in the dictionary to show only items linked to the current PLC selected program:
- Unchecked: All project variables are displayed. This is the default setting.
- Selected: The variables in the Dictionary are filtered to show only those relevant to the PLC item currently selected in the project tree.
- Along with the Global, retains and variables related to the selected program or UDFB, structure definitions are shown.
- The dictionary content changes accordingly if another PLC program is selected in the project tree.
- The columns in the Variables tab can be reordered, resized, and hidden by double clicking on the filter icon in top left corner of the table.
- Sort the list of variables in the table by either:
Press the Spacebar to toggle to the relevant edition mode.
Mode |
Description |
---|---|
One Parameter |
In the cell edition mode, double-click on the parameter. |
All the parameters are at the same time |
In the row edition mode, double-click in any parameter to open the dialog box for variable configuration. See Variables about parameters. |
-
-
A variable cannot be changed when the KAS-IDE Kollmorgen Automation Suite - Integrated Development Environment is connected to the controller.