AOUT.MODE
Description
AOUT.MODE sets the analog output functionality A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances..
Example
You can use AOUT.MODE and AOUT.VALUEU to configure an output signal as follows:
-->AOUT.MODE 0
-->AOUT.VALUEU 5
-->AOUT.VALUEU 4.33
General Information
Type |
NV Parameter |
Units |
N/A |
Range |
0 to 12
|
Default Value |
0 |
Data Type |
Integer |
Start Version |
M_01-00-00-000 |
Variants Supported
*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.