IL.KACCFF

Description

This value sets the gain for the acceleration feedforward (a scaled second derivative of the position command is added to the current command value) .

This parameter is valid only in the position mode (DRV.OPMODE = 2).

General Information

Type

R/W Parameter

Units

mArms/(rad/s²) 

Range

0 to 39113.288 mArms/(rad/s^2)

Default Value

0 mArms/(rad/s²) 

Data Type

Float

See Also

IL.FF

Start Version

M_01-00-00-000

Variant Supported
MKD EtherCAT Yes
AKD-N Yes
MKD-N Yes
MKD-C No
EtherCAT CoE and CANopen
Index/Subindex Object Start Version
3426h/0 M_01-00-00-000

Related Topics

"Current Loop"