IL.KBUSFF
Description
This parameter scales the feedforward term added by the fieldbus An industrial network system for real-time distributed control (e.g., CAN or PROFIBUS, Sercos®). It is a way of connecting instruments in a plant design. to the current command. The nominal feedforward value can be multiplied by this gain value.
This parameter is only used in the position Position means a point in space which is described by different coordinates. Depending on the used system and transformation it can consist of a maximum of six dimensions (coordinates).This means three Cartesian coordinates in space and coordinates for the orientation. In ACS there can be even more than six coordinates. If the same position is described in different coordinate systems the values of the coordinates are different. mode (DRV.OPMODE = 2).
General Information
Type |
NV Parameter |
Units |
NA |
Range |
0 to 2 |
Default Value |
0 |
Data Type |
Float |
See Also |
|
Start Version |
M_01-00-00-000 |
Index Zero pulse (zero signal) of a hardware pin such as digital input or feedback pin./Subindex | Object Start Version |
---|---|
50E2h/0 |
M_01-00-00-000 |
Related Topics