IL.OFFSET

Description

This value is added to the overall current loop feedforward value.

General Information

Type

RW Parameter

Units

A

Range

[IL.LIMITN to IL.LIMITP

Default Value

0 A

Data Type

Float

See Also

IL.FF

Start Version

M_01-00-00-000

Variant Supported
MKD EtherCAT Yes
AKD-N Yes
MKD-N Yes
MKD-C No
EtherCAT CoE and CANopen
Index/Subindex Object Start Version
3423h/0 M_01-00-00-000

Related Topics

"Current Loop"