MOTOR.IPEAK
Description
This parameter configures the drive In electrical engineering, a drive is an electronic device to provide power to a motor or servo. Control device for regulating the speed, torque and position of a motor. A unit controlling a motor using the current and timing in its coils. for the motor An actuator focused to a movement, converting electrical energy in a force or torque.'s peak, instantaneous-rated current. MOTOR.IPEAK is used to limit clamp the magnitude of the torque The tendency of a force to rotate an object about an axis. A force is a push or a pull; a torque is a twist. producing q-component current command (IL.CMD).
-
- This parameter is automatically configured for Kollmorgen motors when AXIS#.MOTOR.AUTOSET = 1 and can be modified while AXIS#.MOTOR.AUTOSET = 1 if its AXIS#.MOTOR.DISAUTOSET index Zero pulse (zero signal) of a hardware pin such as digital input or feedback pin. = 1.
General Information
Type |
NV Parameter |
Units |
mA |
Range |
0.200 to 1,000 A |
Default Value |
2.000 A |
Data Type |
Float |
See Also |
|
Start Version |
M_01-00-00-000 |
Index/Subindex | Object Start Version |
---|---|
358Fh/0 | M_01-00-00-000 |
Related Topics