MOTOR.KT
Description
This parameter is the torque The tendency of a force to rotate an object about an axis.
A force is a push or a pull; a torque is a twist. constant of the motor An actuator focused to a movement, converting electrical energy in a force or torque. in Nm/A.The value can be online checked according to the following equation:
Kt = 60 *√3 * Ui/( 2 * π* n)
Where:
Ui = induced voltage of the motor
n = actual rotor velocity For a group of axes this means: In ACS the velocities of the different axes. In MCS and PCS it provides the velocity of the TCP
-
- This parameter is automatically configured for Kollmorgen motors when AXIS#.MOTOR.AUTOSET = 1 and can be modified while AXIS#.MOTOR.AUTOSET = 1 if its AXIS#.MOTOR.DISAUTOSET index Zero pulse (zero signal) of a hardware pin such as digital input or feedback pin. = 1.
General Information
Type |
NV Parameter |
Units |
Nm/A |
Range |
0.001 Nm/A to 1,000,000.000 Nm/A for rotary motors. 0.001 Nm/A to 1,000,000.000 N/A for linear motors. |
Default Value |
0.1 Nm/A |
Data Type |
Float |
See Also |
N/A |
Start Version |
M_01-00-00-000 |
Index/Subindex | Object Start Version |
---|---|
3593h/0 | M_01-00-00-000 |
Related Topics