PL.FBSOURCE
Description
This parameter determines the feedback source that the position loop uses. A value of 0 for this parameter selects the primary feedback, a value of 1 selects the secondary feedback. If you use the secondary feedback as the source for the position loop, then FB2.MODE mode should be set as 0 (A/B signals). A/B signals are the only supported feedback type as secondary feedback into the position loop. Other settings for FB2.MODE are intended as pulse inputs or a gearing command when PL.FBSOURCE remains 0.
Value | Description |
---|---|
0 |
Primary Feedback connected to X10. |
1 | Secondary Feedback (DRV.HANDWHEEL) connected to X7 or X9. |
2 | Tertiary Feedback connected to X9 (only supported with AKD-x-xxxxx-NBxx-xxxx). |
General Information
Type |
NV Parameter |
Units |
N/A |
Range |
Range will differ depending on drive model. |
Default Value |
0 |
Data Type |
Integer |
Start Version |
M_01-00-00-000 |
Variant | Supported |
---|---|
MKD EtherCAT | Yes |
MKD-N | Yes |
MKD-C | No |
Index/Subindex | Object Start Version |
---|---|
5128h/0 |
M_01-00-00-000 |
Related Topics