FFLD Contacts and Coils
Contacts |
Coils |
---|---|
Negative Transition -|N|- |
Reset New start of the microprocessor. (Unlatch) -(R)- |
Normally Closed -|/|- |
De-energize -(/)- |
Normally closed negative transition -|/N|- |
Negative transition sensing coil -(N)- |
Positive transition sensing coil -(P)- |
|
Normally Open -| |- |
Energize -( )- |
Positive Transition -|P|- |
Set (Latch The control word is used to activate the drive's latch status machine. The latch control word is processed independently of the EtherCAT® bus cycle. The status word is used to return the drive's latch status.) -(S)- |
See Also