Sequential Function Chart (SFC) Editor
The editor supports advanced graphic features such as drag-and-drop, so that you can freely and rapidly arrange the elements of your diagram. It also supports automatic chart formatting when inserting or deleting items, and thus enables Enable signal for the drive, Hardware-Enable with 24V signal to X8, Software-Enable command by setup Software, fieldbus or permanently set. Both are required for enabling the drive. quick input using the keyboard.
-
-
For each step, the cells referring to P1, N, and P0 actions are colored when they are defined.
-
-
- Select a step, transition, or jump and press Ctrl+ENTER to change its number.
- Press the Spacebar on the main corner (on the left) of a ulergence or convergence, to set either double or single horizontal line style.
See (➜ # 1, Sequential Function Chart (SFC)) for more information.