FunctionMLAxisReAlignPipe Network motion icon

Description

When stopping the drive a motion profile is applied to decelerate. During the deceleration, the Reference position changes. Calling MLAxisReAlign realigns the actual position with the reference position by moving the axis by the specified delta position, which is typically calculated by the application code. After a MLAxisStop is executed, a MLAxisReAlign is required for the Pipe Position to be used again (see more details about the Restarting Motion here).

The function returns TRUE if it succeeds.


  • The realign function do not work properly if the MLAxisStop function is continuously executed via its Start input

Arguments

Input

ID

Description

ID Name of the Axis block

 

Data type

DINT

 

Range

 

Unit

n/a

 

Default

Acceleration

Description

Sets the Realign Acceleration

 

Data type

LREAL

 

Range

 

Unit

User unit/sec2

 

Default

Deceleration

Description

Sets the Realign Deceleration rate

 

Data type

LREAL

 

Range

 

Unit

User unit/sec2

 

Default

Speed

Description

Sets the Axis Speed

 

Data type

LREAL

 

Range

 

Unit

User unit/sec

 

Default

DeltaPos

Description

Sets the Axis Delta Position, or the relative distance to be moved

 

Data type

LREAL

 

Range

 

Unit

User unit

 

Default

Output

Default (.Q)

Description

Returns true when function successfully executes

See more details here

 

Data type

BOOL

 

Unit

n/a

Related Functions

MLAxisReAlgnRdy

Example

Structured Text

 

MLAxisReAlign(PipeNetwork.Axis1, 100000, 100000, 500, 20 ) ;

 

Ladder Diagram

MLAxisReAlign: LD example

Function Block Diagram

MLAxisReAlign: FBD example

Go back to the top of the page [Top]