FunctionMLGearReadRatSlpPipe Network motion icon

Description

Returns the Ratio Slope value of a selected Gear Block from the Pipe Network. Ratio Slope sets the limit in 1/Seconds (or s -1) at which step changes in Ratio are implemented.

Arguments

Input

BlockID

Description

ID number of an initialized Gear Pipe Block

 

Data type

DINT

 

Range

[-2147483648, 2147483648]

 

Unit

n/a

 

Default

Output

Slope

Description

The Ratio Slope value currently assigned to the selected Gear Pipe Block, , which may be a different sign than what is programmed with MLGearWriteRatSlp.

 

Data type

LREAL

 

Unit

1/sec (or s -1)

Related Functions

MLGearWriteRatSlp

MLGearInit

Example

Structured Text

//Find the Ratio Slope value of Gear1 Pipe Block
Gear1RatioSlope := MLGearReadRatSlp(PipeNetwork.GEAR1);

Ladder Diagram

MLGearReadRatSlp: LD example

Function Block Diagram

MLGearReadRatSlp: FBD example

Go back to the top of the page [Top]