FunctionMLMstRelPipe Network motion icon

Description

Performs a move for a specified distance relative to the current position. Returns TRUE if the function succeeded.

Arguments

Input

EN

Description

Enables FB to be executed

 

Data type

BOOL

 

Range

0, 1

 

Unit

n/a

 

Default

Block ID

Description

ID name of the Master Block

 

Data type

DINT

 

Range

[-2147483648, 2147483648]

 

Unit

n/a

 

Default

DeltaPos

Description

Relative distance to move

 

Data type

LREAL

 

Range

 

Unit

User unit

 

Default

Output

Default (.Q)

Description

Returns true when function successfully executes

See more details here

 

Data type

BOOL

 

Unit

n/a

Related Functions

MLMstWriteSpeed

MLMstWriteDecel

Example

Structured Text

 

MLMstRel( PipeNetwork.MASTER, 750.0 );

 

Ladder Diagram

MLMstRel: LD example

Function Block Diagram

MLMstRel: FBD example

Go back to the top of the page [Top]