File Path Conventions

Depending upon the system used, paths to file locations may be defined as either absolute (C://dir1/file1) or relative paths (/dir1/file1). Not all systems handle all options, and the paths will vary depending upon the system.

System Absolute Paths Relative Paths Handling of Directories
AKD PDMM or PCMM There is no support for creating directories on the controller. Any path provided to the function blocks, file1 for example, will be appended with the default userdata folder which is:
/mount/flash/userdata
Simulator When a relative path is provided to the function blocks, the path is appended with the default userdata folder, which is:
<User Directory>/Kollmorgen/Kollmorgen Automation Suite/Sinope Simulator/Application/userdata
PAC When a relative path is provided to the function blocks, the path is appended with the default userdata folder, which is:
<User Directory>/Kollmorgen/Kollmorgen Automation Suite/Sinope Runtime/Application/userdata

See Also: