Motion Library - Convertor

Name Description Return type
MLCNVConECAT Connect the output of a pipe convertor block to an EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs Output (Rx) PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. object.  
MLCNVConnect Connects a converter Pipe Block to the specified axis BOOL
MLCNVConnectEx Connects an extra converter Pipe Block to the specified axis. This function connects the output of a pipe to an axis data other than the control position. BOOL
MLCNVDisconnect Disconnects a converter Pipe Block from its associated axis BOOL
MLCNVInit Initializes a converter Pipe Block in Position or Speed mode BOOL