FunctionECATWCStatusPLCopen motion iconPipe Network motion icon

Description

This function returns the current number of working counter errors for the Sync unit. The working counter errors are cleared to zero when the EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs network is taken from Init to OP state.

  • Value 0 means no working counter errors.
  • When the value is non zero, the master will automatically reduce the count by 1 for every thousand good frames received.
  • When the working counter error exceeds the Working Counter Error Limit, the EtherCAT network will be stopped.

Figure 7-197: ECATWCStatus function

Arguments

Input

SyncUnit Description Sync Unit Index (for future compatibility with multiple frames)
  Data type INT
  Range 0
  Unit N/A
  Default -

Output

Count Description Working Counter error
  Data type UDINT
  Unit N/A

Related Functions

ECATDeviceStatus, ECATMasterStatus

Example

Structured Text

(********************************************************)
(* read Ethercat Working counter value *)
(********************************************************)

wcErrorCounter := ECATWCStatus( 0 );

FBD

FFLD

Go back to the top of the page [Top]