Keyword Link IconSearch IndexFile and TCP/IP Function Block ErrorID Output

Following is the list of possible errors that could be returned at the ErrorID ourput of the File Tools Function Blocks and Search IndexTCP/IP Function Blocks.

File Function Block Errors
ErrorID Description
16000 Error opening file.
16001 All PLCClosed "Programmable Logic Controller" A Programmable Logic Controller, PLC, or Programmable Controller is a digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines. Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events file handles used.
16002 File ID is invalid.
16003 File ID has been closed.
16004 Error in file stream.
16005 End of file encountered.
16006 Internal file FB error.
16007 Unknown file error.
16008 No such file or directory.
16009 Bad file descriptor.
16010 File already exists.
16011 Too many open files in the system.
16012 Text file is busy.
16013 File is too large.
16014 File system is read only.
16015 File locking deadlock.
16016 Filename is too long.
16017 File positioning error.
16018 Bad or corrupted file system detected .
TCP/IP Function Block Errors
ErrorID Description
16100 Connection error.
16101 TCP ID has been closed.
16102 All PLC TCP handles used.
16103 TCP ID is invalid.
16104 Failed to allocate TCP/IP socket.
16105 TCP operation internal error.