Motion Library - Sampler

Name Description Return type
MLSmpConECAT Connects a sampler block to the specified CoE object in a PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. BOOL
MLSmpConnect Connects a sampler block to a pipe network axis or pipe block BOOL
MLSmpConPLCAxis Connects a sampler block to a PLCopenClosed A vendor -and product- independent worldwide association active in Industrial Control and aiming at standardizing PLC file formats based on XML axis variable BOOL
MLSmpConPNAxis Connects a sampler block to a Pipe Network axis variable BOOL
MLSmpInit Initializes a sampler object BOOL