Add Comments to Pipe Network

To add a comment:

  1. Right-click on the Pipe Network editor's background and select the Add Comment command in the menu
  2. Right-click on the comment opens the contextual menu to let you edit (Properties command) or delete the comment

Figure 4-13: Pipe Network comments: editing, and deselected.

Click and drag the gray bar to move the comment.