Create the PipeNetwork

To create the PipeNetwork, do as follows:

  1. In the Project Explorer, double-click the PipeNetwork button to open the graphical PipeNetwork Editor.

    Pipe Network - Open Editor

  2. Figure 4-5: PipeNetwork - Open Editor


    • If you have created a project from a template (for instance the standard two-axis template) there is already a PipeNetwork in the editor.

  3. To add a new Pipe Block, right-click on the editor's background and select the Add Pipeblock command in the menu
  4. Choose in the drop-down menu the type of Pipe Block you want to add

    Pipe Network - Add Pipeblock

  5. Figure 4-6: PipeNetwork - Add Pipeblock

    For more details on Pipe Blocks, refer to Pipe Block and Pipe Blocks Description.

  6. To link the newly created Pipe Block, move the arrow to the corresponding Pipe Block with a drag-and-drop operation

    Pipe Network - Create a Link

  7. Figure 4-7: PipeNetwork - Create a Link