Edit Properties of Pipe Blocks

Initial values for Pipe Network blocks are entered in the parameter screen for each block. To get to the parameter screen, right-click on a Pipe Block and select the Properties command in the contextual menu.

  • Right-click on the Pipe Block and select the Properties command in the menu

    Pipe Network - Pipe Block Properties

    Figure 4-11: Pipe Network - Pipe Block Properties

  • The Properties window can also be opened by selecting the block and pressing Alt+Enter.

You can change the name (or even the type of Pipe Block) in the General tab.

The Parameters tab gives access to properties related to the type of Pipe Block (for more details, refer to Pipe Blocks Description).