EtherCAT Devices tab

The EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs Devices tab lists all the EtherCAT devices and provides for the ability to discover and map their use. The interface is slightly different for AKD and AKD2G drives. The AKD2G prompts you to select the mapping by the drive axis.

EtherCAT Summary Form

Figure 4-104: EtherCAT Devices Summary Form

First generation AKD drives support one axis per drive, while AKD2G drives support two axes per drive. When configuring drives in the EtherCAT Devices tab, you will need to designate which motion axis applies to each "drive axis", which is the actual axis the drive controls.

Item Description
Show only drives This option hides from the list all EtherCAT slaves that are not drives
Scan Devices The KAS RuntimeClosed In computer science, runtime (or run-time) describes the operation of a computer program, the duration of its execution, from beginning to termination (compare compile time). Within KAS, runtime also refers to the virtual machine that manage the program written in a computer language while it is running sends EtherCAT messages to discover the physical devices and modules present in the network (see explanation below)
Name, Vendor, Product, and Model The project device name, vendor name, product name (or code number), and model number for each device is displayed and ordered by the position in the tree. The model (when available) includes the extension and connectivity options, NBEC for example. See AKD Models and AKD2G Models for information on interpreting the model text of Kollmorgen drives.
FW Version

For Kollmorgen drives, the firmware version is displayed on the conditions that: 

For other devices, the firmware version is displayed if the Scan Devices routine was successfully run and the device supports reading this informaiton over EtherCAT (i.e. it uses CoE object 0x100A:0).

Otherwise (Unknown) is displayed.

  •  
  • If a Kollmorgen drive is showing the firmware version as "Unknown", the drive has valid resident firmware (from which to boot), but does not have valid operational firmware. Please download and install the latest operational firmware and reboot the AKD/AKD2G.
Drive Axis Number This number designates which axis, of those available on a drive, is being defined. For most drives, this number will just be a "1", but for AKD2Gs, there are two entries, Drive Axis Number 1 and Drive Axis Number 2,
Mapped to Axis

For each drive, it is displayed if it is:

Simulated

Select this option when you want to simulate the device, which means that the device is not used and no communication to this device is performed through the fieldbus.

Save parameters to NV memory

Allows you to save the drives' parameters to the NVRAM of each drive currently selected in the list. This action is enabled only when the Online Mode is activated

You will be automatically be prompted with the option to save modified drive parameters if this action has not been performed prior to the following circumstances.

Upgrade Firmware

This command triggers a firmware upgrade for the selected drives (you can use Ctrl+A shortcut to select all drives).

For more details, refer to FAQ section.

Table 4-23: EtherCAT Devices

Scan Devices

The scan process allows the following tasks:

Figure 4-105: EtherCAT Network - Physical View

EtherCAT Network - Logical View

Figure 4-106: EtherCAT Network - Logical View. K-Bus on left, E-Bus on right

During the scan operation, all physical devices connected to the EtherCAT network will be discovered and identified. The KAS IDE will list the devices in the order they are connected. Kollmorgen devices, which include AKD and S300Closed "Servostar 300 drive" See Servo Drive in Glossary/S700Closed "Servostar 700 drive" See Servo Drive in Glossary drives, Standard I/O Couplers, and remote I/O terminals (for a list, see "Remote Input/Output Terminals") will include detailed information for each device.

The status of devices can be determined by their icon in the logical view.

Icon Meaning Description
(device icon) Normal The device has been added by scanning the system. The associated ESI file has been found. The icon varies by device, but is the icon set by the manufacturer in the ESI file.
Excluded The device has been added manually or has been disassociated from a discovered device.
ESI missing The ESI file is missing.
Error For AKD, shown when there is an error.

Table 4-24: EtherCAT device icon descriptions.

Scan Limitations

  • I/O slices for Standard I/O Coupler do not reveal their Device IDs.
  • The discovery feature does not differentiate between AKT-DN-004-000 and AKT-DNH-004-000 I/O terminals. Nor between AKT-DN-008-000 and AKT-DNH-008-000.
  • Devices other than those made by Kollmorgen will be identified by the Vendor Name (or ID number) and Product Name (or ID number). If the device is missing an ESI file, then you will need to import the ESI file supplied by the device Vendor. The ESI file is required by the IDE to decode and display the Product Name, Device Description, and other details.
  • ESI files for any MDP devices connected ot the network should be added to KAS IDE's ESI library before starting a scan. If the ESI file for an MDP device is not available, then the scan cannot identify the device and cannot discover any physical or logical modules under the device.

Concept Link IconSee Also