AKD Backup/Restore Compatibility

The replacement AKD or AKD2G must have the same model number as the device that was originally stored in the backup. The Restore operation compares the model numbers between the backup and the replacement AKD. The restore will not be allowed if they are not compatible.


  • The "AKD-Pxxxxx-NB" models are functionally compatible with, and may be replaced with "AKD-Pxxxxx-NC" devices provided the backup contains AKD firmware version v01-20-00-003 or later.
      Restore
      NBNC
    BackupNB
    NC

  • The serial number (SN) is displayed in the Physical topology web server view and on the sticker affixed to the AKD. You can use the serial number to match the actual hardware with its representation on the web server.