Plugging a probe from the Pipe Network

A probe (variable) can be directly plugged or mapped to the Oscilloscope from the Pipe Network:

  1. Right-click on a Pipe Block
  2. Select Plug on channel… in the menu

    Plugging a Probe from the Pipe Network
  3. Figure 6-35: Plugging a Probe from the Pipe Network

  4. Define the probe parameters.

  5. Field Description
    Name Variable's name
    Type Variable's type
    Channel Channel's number where the variable has to be plugged
    Data Desired variable information to show (the list depends on the type of Pipe Block. See Pipe Blocks Description for more details)
    Derivation order Performs a derivation of the measurement of the selected variable. If this value is different from 0, the derived value of the selected order is shown on the selected channel
    Derivation Period Specifies the modulo period for a periodic variable to remove spikes in the display of derivative orders greater than zero. The value entered should either be 0.0 (No Modulo) or the Modulo Period (eg. 360.0).