PDMM/PCMM EDS file for EtherNet/IP

The KAS installation contains an EtherNet/IP EDS file for the Kollmorgen controller. This file may be needed by other controllers, (PLCs, PCs etc.) to configure the EtherNet/IP communication with a AKD PDMM.

The KAS_Controller_EIP.eds file is located in the \Astrolabe\Bin\EDS directory, where the KAS software was installed. By default, the EDS file is located:

C:\Program Files (x86)\Kollmorgen\Kollmorgen Automation Suite\Astrolabe\Bin\EDS\KAS_Controller_EIP.eds
Revision Compatibility Change
1.0 KAS v2.7 only Initial revision
1.1 KAS v2.8 only Updated vendor information
1.2 KAS v2.9 only Support up to 4 input and output assemblies when KAS RuntimeClosed In computer science, runtime (or run-time) describes the operation of a computer program, the duration of its execution, from beginning to termination (compare compile time). Within KAS, runtime also refers to the virtual machine that manage the program written in a computer language while it is running is configured as adapter (server), up from 1.

Table 7-3: Revision history for AKD PDMM EDS file for EtherNet/IP