Safety Terminal Reaction Times

The safety terminals form a modular safety system that exchanges safety-oriented data via the Safety-over-EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs protocol. This topic is intended to help you determine the system's reaction time from the change of signal at the sensorClosed A sensor is a type of transducer that converts one type of energy into another for various purposes including measurement or information transfer to the reaction at the actuatorClosed A mechanical device for moving or controlling a mechanism or system. An actuator typically is a mechanical device which transforms an input signal (usually an electrical signal) into motion.

Typical Reaction Time

The typical reaction time is the time that is required to transmit information from the sensor to the actuator, if the overall system is working without error in normal operation.

Figure 7-302: Typical reaction time

Definition Description

RTSensor

Reaction time of the sensor until the signal is provided at the interface. Typically supplied by the sensor manufacturer.

RTInput

Reaction time of the safe input, such as AKT2G-SDI-004. This time can be found in the technical data. In the case of the AKT2G-SDI-004 it is 4 ms.

RTComm

Reaction time of the communication This is typically 3x the EtherCAT cycle time, because new data can only be sent in a new Safety-over-EtherCAT telegram. These times depend directly on the higher-level standard controller (cycle time of the PLCClosed "Programmable Logic Controller" A Programmable Logic Controller, PLC, or Programmable Controller is a digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines. Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events).

RTLogic

Reaction time of the logic terminal. This is the cycle time of the safety PLC, depending on the size of the safety project.

RTOutput

Reaction time of the output terminal. This typically lies within the range of 2 to 3 ms.

RTActor

Reaction time of the actuator. This information is typically supplied by the actuator manufacturer

WDComm

Watchdog time of the communication

This results in the following equation for the typical reaction time:

with, for example

Worst-Case Reaction Time

The worst case reaction time is the maximum time required to switch off the actuator in the case of an error.

Figure 7-303: Worst-case reaction time

This assumes that a signal change occurs at the sensor and is transmitted to the input. A communication error occurs at precisely the moment when the signal is to be transferred to the communication interface. This is detected by the logic following the watchdog time of the communication link. This information should then be transferred to the output, but a further communication error occurs here. This error is detected at the output following the expiry of the watchdog time and leads to the switch-off.

This results in the following equation for the worst-case reaction:

with, for example