DOUT.STATES

Description

DOUT.STATES reads the states of the digital output. The leftmost bit represents DOUT1 and the rightmost bit represents DOUT2.


  • AKD-C only reads the state of DOUT1.

General Information

Type

R/O Parameter

Units

N/A

Range

0 to 11

Default Value

N/A

Data Type

String

BASIC: Integer

Start Version

M_01-00-00-000

Related Topics

Digital Outputs