PL.ERR

Description

PL.ERR reads the position error present when the drive is controlling the position loop. PL.ERR is the difference between the actual position of the motor shaft (PL.FB ) and the commanded position of the drive (PL.CMD ).  If the drive is not in the position operating mode (DRV.OPMODE = 2), then the PL.ERR value is not generated by the drive and this parameter is read as 0.

AKD BASIC Notes


  • When you enable the position error interrupt (by setting INTR.PL.ERR=1), the Position Error fault is disabled. In situations where it would have occurred, a position error interrupt is generated instead.

General Information

Type

R/O Parameter

Units

counts, rad, deg, (custom units)

Range

N/A  

Default Value

N/A

Data Type

Float

BASIC: Integer

See Also

PL.FB

Start Version

M_01-00-00-000

FieldbusClosed A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

/0

/0

M_01-00-00-000

Related Topics

PL.ERRFTHRESH | PL.ERRMODE | PL.ERRWTHRESH

Position Loop