ANY_TO_SINT / ANY_TO_USINTPLCopen motion icon

Operator - Converts the input into a small (8 bit) integer value (can be unsigned with ANY_TO_USINT).

Inputs

IN : ANY  Input value

Outputs

Q : SINT  Value converted to a small (8 bit) integer

Remarks

For BOOL input data types, the output is 0 or 1. For REAL input data type, the output is the integer part of the input real. For TIME input data types, the result is the number of milliseconds. For STRING inputs, the output is the number represented by the string, or 0 if the string does not represent a valid number. In FFLD language, the conversion is executed only if the input rung (EN) is TRUE. The output rung (ENO) keeps the same value as the input rung. In ILClosed "Instruction list" This is a low-level language and resembles assembly Language, the ANY_TO_SINT function converts the current result.

ST Language

Q := ANY_TO_SINT (IN);

FBD Language

FFLD Language

(* The conversion is executed only if EN is TRUE *)
(* ENO keeps the same value as EN *)

IL Language

Op1: FFLD  IN
     ANY_TO_SINT
     ST  Q

See also

ANY_TO_BOOL   ANY_TO_INT   ANY_TO_DINT   ANY_TO_LINT   ANY_TO_REAL   ANY_TO_LREAL   ANY_TO_TIME   ANY_TO_STRING