MLAxisGenIsRdy

Pipe Network motion icon

 FunctionClosed A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Check if an axis is ready. Returns TRUE if the internal generator axis is ready.

Arguments

Input

ID

Description

ID Name of the Axis block

 

Data type

DINT

 

Range

 

Unit

N/A

 

Default

Output

Default (.Q)

Description

Returns true when function successfully executes.

See Function - General Rules for more information.

 

Data type

BOOL

 

Unit

N/A

Related Functions

MLAxisGenIsEN

MLAxisStatus

Example

See Usage Example of Axis Functions for additional examples.

Structured Text

 

MLAxisGenIsRdy(PipeNetwork.Axis1 );

 

Ladder Diagram

MLAxisGenIsRdy: LD example

Function Block Diagram

MLAxisGenIsRdy: FBD example