MLAxisInit

Pipe Network motion icon

 FunctionClosed A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Initializes an axis object.

Input

AxisID

Description

ID Name of the Axis block

 

Data type

DINT

 

Range

 

Unit

N/A

 

Default

ModuloPosition

Description

Value of the period of a cyclic system expressed in user units. The parameter is defined to correctly manage the periodicity (modulo) of the input values.

 

Data type

LREAL

 

Range

 

Unit

User unit

 

Default

UserUnitPerTurn

Description

Define the unit which is equivalent to one revolution of the physical motor.

 

Data type

LREAL

 

Range

 

Unit

N/A

 

Default

FeedbackUnitPerTurn

Description

 
 

Data type

DINT

 

Range

 

Unit

N/A

 

Default

Speed

Description

Sets the Axis Speed

 

Data type

LREAL

 

Range

 

Unit

User unit

 

Default

Acceleration

Description

Sets the Axis Acceleration value

 

Data type

LREAL

 

Range

 

Unit

User unit/sec2

 

Default

Deceleration

Description

Sets the Axis Deceleration value

 

Data type

LREAL

 

Range

 

Unit

User unit/sec2

 

Default

InitialPosition

Description

Initial position value expressed in user logical units. Used only at the pipe activation to initialize the position starting point

 

Data type

LREAL

 

Range

 

Unit

User unit

 

Default

Modulo

Description

Define the mode which can be Modulo (True) or not (False)

 

Data type

BOOL

 

Range

0, 1

 

Unit

N/A

 

Default

Output

Default (.Q)

Description

Returns true when function successfully executes

See Function - General Rules for more information.

 

Data type

BOOL

 

Unit

N/A

Remarks

  • Returns TRUE if the function succeeded.
  • The axis object can be mapped to servo or stepper drives.

FBD Language

MLAxisInit: FBD example

FFLD Language

MLAxisInit: LD example

ST Language

MLAxisInit( PipeNetwork.Axis1, 360.0, 360.0, SHL(1,20), 500.0, 100000.0, 100000.0, 0.0, true ) ;