MLAxisReAlgnRdy

Pipe Network motion icon

 FunctionClosed A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Check if an axis is ready.

Returns TRUE if the internal realignment axis is ready.

Arguments

Input

ID

Description

ID Name of the Axis block.

 

Data type

DINT

 

Range

 

Unit

N/A

 

Default

Output

Default (.Q)

Description

Returns true when function successfully executes.

See Function - General Rules for more information.
 

Data type

BOOL

 

Unit

N/A

Related Functions

MLAxisReAlign

Example

Structured Text

 

MLAxisReAlgnRdy(PipeNetwork.Axis1 ) ;

 

Ladder Diagram

MLAxisReAlgnRdy: LD example

Function Block Diagram

MLAxisReAlgnRdy: FBD example

Go back to the top of the page[Top]