MLAxisReadUUnits

Pipe Network motion icon

 FunctionClosed A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Get the User units per revolution value of the axis.

Arguments

Input

AxisID

Description

ID Name of the Axis block.

 

Data type

DINT

 

Range

 

Unit

N/A

 

Default

Output

OK

Description

Returns true when function successfully executes.

See Function - General Rules for more information.
 

Data type

BOOL

 

Unit

N/A

UserUnitsPerRev

Description

Returns the Axis User Units per revolution.

 

Data type

LREAL

 

Unit

N/A

Example

Structured Text

 

Axis1_User_Units := MLAxisReadUUnits(PipeNetwork.Axis1 ) ;

 

Ladder Diagram

MLAxisReadUUnits: LD example

Function Block Diagram

MLAxisReadUUnits: FBD example

Go back to the top of the page[Top]