MLAxisWritePipPos

Pipe Network motion icon

 FunctionClosed A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Force the pipe position internal value.

This function is working only when no pipe is connected.

Arguments

Input

AxisID

Description

ID Name of the Axis block.

 

Data type

DINT

 

Range

 

Unit

N/A

 

Default

PipePosition

Description

Sets the Axis Pipe Position.

 

Data type

LREAL

 

Range

 

Unit

User unit

 

Default

Output

Default (.Q)

Description

Returns true when function successfully executes

See Function - General Rules for more information.
 

Data type

BOOL

 

Unit

N/A

Related Functions

Example

Structured Text

 

MLAxisWritePipPos(PipeNetwork.Axis1, 3000 ) ;

 

Ladder Diagram

MLAxisWritePipPos: LD example

Function Block Diagram

MLAxisWritePipPos: FBD example

Go back to the top of the page[Top]