MLBlkReadModPos

Pipe Network motion icon

 FunctionClosed A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Get the value of the period of a block in user units.

Inputs

Input

Data Type

Range

Unit

Default

Description

ID

DINT

-2147483648 to 2147483648

N/A

No default

ID number of a created Pipe Block.

Outputs

Output

Data Type

Range

Unit

Default

Description

ModuloPosition

LREAL

N/A

User unit

No default

Current period value for selected Pipe Block.

Remarks

  • The output value of a block is reset each time it reaches its period value.

MLBlkReadModPos

Figure 7-76: MLBlkReadModPos

FBD Language

MLBlkReadModPos: FBD example

FFLD Language

MLBlkReadModPos: LD example

ST Language

//Return and save the Period of a Pipe Block 
GearPeriod := MLBlkReadModPos( PipeNetwork.MyGear );

See Also