Function BlockMC_GrpStopPLCopen motion iconPipe Network motion icon

Description

MC_GrpStop performs a controlled motion stop of all axes in the group. When the path velocity reaches zero any queued moves are flushed from the buffer and the Done output is set. When both the Done output is true and the application has cleared the Execute input the state transitions to GroupStandby. MC_GrpStop can not be aborted.


  • MC_GrpStop does NOT prevent a single axis from executing nor does it prevent other Coordinated Motion moves from executing once MC_GrpStop has completed.

Related Functions

MC_GrpHalt, MC_ErrorDescription

See Coordinated Motion, the top-level topic for Coordinated Motion.

Arguments

For more details on how inputs and outputs work, refer to Function Blocks - General Rules.

Input

Execute Description On the rising edgeClosed A rising edge is the transition of a digital signal from low to high. It is also called positive edge the command to stop all of the axes in the group is initiated.
  Data type BOOL
  Range 0, 1
  Unit N/A
  Default
AxesGroup Description The axes group in which the axes will be stopped.
  Data type AXES_GROUP_REF
  Range N/A
  Unit N/A
  Default
Deceleration Description The path deceleration rate for all of the axes in the group
  Data type LREAL
  Range

0 < Deceleration

See Limitations on Acceleration and Jerk for more information.

  Unit N/A
  Default
Jerk Description Not supported
  Data type LREAL
  Range

0 ≤ Jerk

See Limitations on Acceleration and Jerk for more information.

  Unit N/A
  Default

Output

Done Description If True, then the command completed successfully.
  Data type BOOL
Busy Description TRUE from the moment the EXECUTE input is TRUE until the stop is complete.
  Data type BOOL
Active Description If True, then the stop is still executing.
  Data type BOOL
Error Description If True, an error has occurred.
  Data type BOOL
ErrorID Description Indicates the error identifier if Error output is set to TRUE. See table in PLCopen Function Block ErrorID Output.
  Data type INT

Example

Structured Text

Inst_MC_GrpStop ( EnableStop, Group1_Ref, Deceleration, Jerk );

IL

            BEGIN_ILClosed "Instruction list"
This is a low-level language and resembles assembly
     CAL Inst_MC_GrpStop ( EnableStop, Group1_Ref, Deceleration, Jerk )
END_IL

FBD

FFLD

Go back to the top of the page[Top]