Function BlockECATWriteSDOPLCopen motion iconPipe Network motion icon

Description

This function block writes a 32-bit word to I/O nodes using a CANopen SDO write command.

See EtherCAT Function Blocks That Work With SDOs for information about function blocks which are used to work with drive or remote I/O parameters that are not supported by ML and MC function blocks.

ECATWriteSdo.png

Figure 7-198: ECATWriteSdo

,

State Diagram

ECATWriteSdo State diagram

Figure 7-199: ECATWriteSdo State Diagram

Arguments

Input

Execute Description On the rising edgeClosed A rising edge is the transition of a digital signal from low to high. It is also called positive edge of Execute, an SDO write command will be issued. The function block will only handle one SDO command at a time. If Execute is toggled quickly so that another rising edge occurs before the SDO command has completed, the function block will not issue a second SDO command.
  Data type BOOL
  Range 0, 1
  Unit N/A
  Default
Index Description

The object directory index of the data to be written to.

For more details, refer to:

  • Communication SDOs
  • Manufacturer specific SDOs
  • Profile specific SDOs

To read/write an SDO object with an index greater than 16#7FFF (32767), the value must be entered in the form any_to_int(index # in hex format). For example any_to_int(16#8321).

  Data type INT
  Range
  Unit N/A
  Default
Subindex Description

The sub-index of the object directory variable to be written to.

For more details, refer to:

  • Communication SDOs
  • Manufacturer specific SDOs
  • Profile specific SDOs

To read/write an SDO object with an index greater than 16#7FFF (32767), the value must be entered in the form any_to_int(index # in hex format). For example any_to_int(16#8321).

  Data type SINT
  Range
  Unit N/A
  Default
Size Description The size (number of bytes) to write.
  Data type SINT
  Range 1 - 4
  Unit N/A
  Default
DeviceAddress Description

The EtherCAT address of the device from which data will be written to.

The first node usually has the value '1001'. The second node usually has the value '1002'.

Alternately, use the members of the EtherCAT structure to specify a drive's address to Create Variables.
creating an EtherCAT variable

  Data type INT
  Range
  Unit N/A
  Default
Value Description The value to write to the object directory variable.
  Data type DINT
  Range [-2147483648, 2147483648]
  Unit N/A
  Default

Output

Done Description Indicates whether the SDO call has completed without error.
  Data type BOOL
  Unit N/A
Error Description Indicates whether the SDO call has completed with error:
  Data type BOOL
  Unit N/A
ErrorID Description The SDO call error result, if Error is TRUE (see list of Error Codes in table below). Upon success, Error is set to zero.
  Data type DINT
  Unit N/A

EtherCAT Error Codes

List of EtherCAT Error Codes

Error Code

Value dec (hex)

Description

ECERR_OK

0

The SDO call succeeded

ECERR_DEVICE_ERROR

1792 (0x700)

EtherCAT device is not accessible

ECERR_DEVICE_INVALIDCMD

1794 (0x702)

Invalid mailbox command

ECERR_DEVICE_INVALIDINDEX

1795 (0x703)

An invalid value for the Index input was specified

ECERR_DEVICE_INVALIDACCESS

1796 (0x704)

Reading of the variable is not permitted

ECERR_DEVICE_INVALIDSIZE

1797 (0x705)

An invalid size for the parameter was specified

ECERR_DEVICE_INVALIDDATA

1798 (0x706)

Invalid parameter value(s) in SDO index and/or sub-index

ECERR_DEVICE_NOTREADY

1799 (0x707)

Device is not in a ready state, network is not in operational

ECERR_DEVICE_BUSY

1800 (0x708)

Device is not available to respond

ECERR_DEVICE_INVALIDCONTEXT

1801 (0x709)

Device responded with an illegal error code, indicating the command is not allowed under the present conditions

ECERR_DEVICE_NOMEMORY

1802 (0x70A)

EtherCAT mailbox is out of memory or device is out of disk space

ECERR_DEVICE_INVALIDPARM

1803 (0x70B)

EtherCAT mailbox request was not valid

ECERR_DEVICE_NOTFOUND

1804 (0x70C)

EtherCAT device not found

ECERR_DEVICE_SYNTAX

1805 (0x70D)

An unexpected error occurred

ECERR_DEVICE_INVALIDSTATE

1810 (0x712)

The EtherCAT device is in an invalid state

ECERR_DEVICE_TIMEOUT

1817 (0x719)

The EtherCAT device failed to respond, timing out

ECERR_DEVICE_INSERTMAILBOX

1826 (0x722)

Error while inserting the mailbox command into internal FIFO

ECERR_DEVICE_INVALIDOFFSET

1827 (0x723)

An invalid value for the SubIndex input was specified

ECERR_DEVICE_UNKNOWNMAILBOXCMD

1828 (0x724)

The master sent an unknown mailbox command to the slave

ECERR_DEVICE_ACCESSDENIED

1829 (0x725)

Device responded with an invalid access error code, indicating the command is not allowed

ECERR_DEVICE_INVALIDADDR

1832 (0x728)

Can’t send a mailbox command to the specified slave

ECERR_DEVICE_NOT_A_FSOE_MASTER

1836 (0x72c)

Device is not a FSoE master.

ECERR_DEVICE_PARAM_ACCESS_ERROR

1920 (0x780)

Unknown error occurred while accessing parameter

ECERR_DEVICE_PARAM_NOT_FOUND

1921 (0x781)

Parameter was not found

ECERR_DEVICE_PARAM_NOT_INTEGER

1922 (0x782)

Parameter is a floating-point value. Integer value required.

ECERR_DEVICE_VALUE_IS_NEGATIVE

1923 (0x783)

No negative values allowed. Value specified was negative.

ECERR_DEVICE_VALUE_OUT_OF_RANGE

1924 (0x784)

Value is out of data-range

ECERR_DEVICE_VALUE_GREATER_THAN_MAX

1925 (0x785)

Value bigger than maximum

ECERR_DEVICE_VALUE_LOWER_THAN_MIN

1926 (0x786)

Value lower than minimum

ECERR_CLIENT_ERROR

2048 (0x800)

Error in Mailbox response to a previously sent mailbox command

ECERR_CLIENT_TIMEOUT

2049 (0x801)

The SDO command timed out

ECERR_CLIENT_ INVALIDPARM

2050 (0x802)

An invalid value was specified

ECERR_CLIENT_ INVALIDSIZE

2051 (0x803)

An invalid value for the size input was specified

Related Functions

ECATReadSDO

Example

Structured Text

      (* Write 58.000 to PL.KP of first AKD D
      rive on Ethe
      rCAT network *)
Inst_ECATWriteSdo( TRUE, 16#3542, 0, 4, 1001, 58000 );

 

      (* Write a value of 246 to the 4 byte data in SDO index 8321h (33569 decimal), sub-index 1 on the first AKD Drive *)
Inst_ECATWriteSdo( TRUE, any_to_int(16#8321), 1, 4, 1001, 246 );

FBD

FFLD

See also the FAQ to set the update rate for SDO communication.

Go back to the top of the page[Top]