MC_InitAxisFeedback

PLCopen motion icon

 FunctionClosed A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - initializes a PLCopenClosed A vendor -and product- independent worldwide association active in Industrial Control and aiming at standardizing PLC file formats based on XML Digitizing Axis position data.

A call to this function is automatically generated when the application is compiled, based on the data entered in the PLCopen Axis Data dialog.

Figure 7-122: MC_InitAxisFeedback

Arguments

See Function Blocks - General Rules for more information about how inputs and outputs work.

Input

En

Description

Request to Initialize a PLCopen Digitizing Axis.

This input is only applicable to FFLD programs.

 

Data type

BOOL
 

Range

0,1
 

Unit

N/A
 

Default

-

AxisNumber

Description

Digitizing Axis Number
 

Data type

UINT
 

Range

[1,256]
 

Unit

none
 

Default

-

FeedbackPDOIndex

Description

The object Index through which the feedback data is sent.
 

Data type

UINT
 

Range

[0,65536]
 

Unit

N/A
 

Default

-

FeedbackPDOSubIndex

Description

The sub index of the object through which the feedback data is sent to controller.
 

Data type

UINT
 

Range

[0,255]
 

Unit

 
 

Default

 

FeedbackDataResolution

Description

The resolution of the Encoder
 

Data type

UINT
 

Range

[1,32]
 

Unit

N/A
 

Default

-

Output

OK

Description

Indicates the initialization is complete. This output is only applicable to FFLD programs.

See Function - General Rules for more information.

 

Data type

BOOL

ErrorID

Description

Indicates if the call failed or succeeded. If the call succeeds, will be set to 0.
 

Data type

DINT

Example

Structured Text

(* MC_InitAxisFeedback STClosed "Structured text"
A high-level language that is block structured and syntactically resembles Pascal example *)
// Initialize the digitizing Axis (Axis #3) with the Feedback object 0x60E4 subIndex 2.
Encoder resolution is 25bits.
ErrID := MC_InitAxisFeedback(3, 16#60E4, 16#02, 25);

FBD Example