Function BlockMC_MoveRelativePLCopen motion icon

Description

This function block executes a single-axis move for a specified distance to perform incremental motion.

MC_MoveRelative

Figure 7-138: MC_MoveRelative

Time Diagram

This image is an example of the combination of two relative move FunctionClosed A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. Blocks.

  • The left part of the timing diagram illustrates the case if the Second Function BlockClosed A function block groups an algorithm and a set of private data. It has inputs and outputs. is called after the First one.
    • If First reaches the commanded distance 6000 (and the velocity is 0), then the output Done causes the Second FB to move to the distance 10000.
  • The right part of the timing diagram illustrates the case if the Second move Function Blocks starts the execution while the First FB is still executing.
    • In this instance, the First motion is interrupted and aborted by the Test signal during the constant velocity of the First FB.
    • The Second FB adds on the actual position of 3250 the distance 4000 and moves the axis to the resulting position of 7250.

Figure 7-139: Time Diagrams: First and Second FBs

MC_MoveRelative: Timing Diagram

Figure 7-140: Time Diagram

Arguments

See Function Blocks - General Rules for more information about how inputs and outputs work.

Input

Execute

Description

Requests to queue the move.

 

Data Type

BOOL

 

Range

0, 1

 

Unit

N/A

 

Default

Axis

Description

Name of a declared instance of the AXIS_REF library function.

See Axis Name and Number for more information.

 

Data Type

AXIS_REF

 

Range

[1,256]

 

Unit

N/A

 

Default

Distance

Description

Distance

 

Data Type

LREAL

 

Range

 

Unit

User unit

 

Default

Velocity

Description

Velocity setpointClosed Setpoint is the target value that an automatic control system, for example PID controller, will aim to reach

 

Data Type

LREAL

 

Range

 

Unit

User unit/sec

 

Default

Acceleration

Description

Trapezoidal: Acceleration rate

S-curve: Maximum acceleration

 

Data Type

LREAL

 

Range

 

Unit

User unit/sec 2

 

Default

Deceleration

Description

Trapezoidal: Deceleration rate

S-curve: Unused

 

Data Type

LREAL

 

Range

 

Unit

User unit/sec 2

 

Default

JerkClosed In physics, jerk is the rate of change of acceleration; more precisely, the derivative of acceleration with respect to time

Description

Trapezoidal: 0

S-curve: Constant jerkClosed In physics, jerk is the rate of change of acceleration; more precisely, the derivative of acceleration with respect to time

 

Data Type

LREAL

 

Range

 

Unit

User unit/sec 3

 

Default

BufferMode

Description

0 = abort

1 = buffer

2 = blend to active

3 = blend to next

4 = blend to low velocity

5 = blend to high velocity

See the table in Buffer Modes.

 

Data Type

SINT

 

Range

[0,5]

 

Unit

N/A

 

Default

Output

Done

Description

Indicates the move completed successfully.
The Command Position has reached the endpoint.

 

Data Type

BOOL

Busy

Description

High from the moment the Execute input is one-shot to the time the move is ended.

 

Data Type

BOOL

Active

Description

Indicates this move is the active move.

 

Data Type

BOOL

CommandAborted

Description

Indicates the move was aborted.

 

Data Type

BOOL

Error

Description

Indicates an invalid input was specified or the move was terminated due to an error.

 

Data Type

BOOL

ErrorID

Description

Indicates the error if Error output is set to TRUE.

See the table in PLCopen Function Block ErrorID Output.

 

Data Type

INT

Example

Structured Text

(* MC_MoveRelative ST example *)

Inst_MC_MoveRelative( MovRelReq, Axis1, 10.0, 200.0,150.0, 150.0, 0,0 );

MovRelDone := Inst_MC_MoveRelative.Done; //store Done output into user defined variable

See Main for more information about how this function is used in the Hole punch project.

Ladder Diagram

MC_MoveRelative: LD example

Go back to the top of the page[Top]