MLMstWriteSpeed

Pipe Network motion icon

 FunctionClosed A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Set the speed of motion for the MLMstAbs and MLMstRel blocks.

  • Returns TRUE if the function succeeded.
  • This function does not generate any motion.

Arguments

Input

EN Description Enables FB to be executed
  Data type BOOL
  Range 0, 1
  Unit N/A
  Default
Block ID Description ID name of the Master Block
  Data type DINT
  Range [-2147483648, 2147483648]
  Unit N/A
  Default
Speed Description Speed of the motion
  Data type LREAL
  Range
  Unit User unit/sec
  Default

Output

Default (.Q) Description Returns true when function successfully executesSee Function - General Rules for more information.
  Data type BOOL
  Unit N/A

Related Functions

MLMstWriteDecel

Example

Structured Text

 

MLMstWriteSpeed( PipeNetwork.MASTER, 400.0 );

 

Ladder Diagram

MLMstWriteSpeed: LD example

Function Block Diagram

MLMstWriteSpeed: FBD example

Go back to the top of the page[Top]