MLPmpInit

Pipe Network motion icon

 FunctionClosed A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Initializes a Pmp Block for use in a PLCClosed "Programmable Logic Controller" A Programmable Logic Controller, PLC, or Programmable Controller is a digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines. Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events Program.

This function block is automatically called by the Function PipeNetwork(MLPN_CREATE_OBJECTS) if a Pmp Block is added to the Pipe Network, with user-defined settings entered in the Pipe Blocks Properties screen.

The Pmp Pipe Block is assigned a Name, SAMPLING_PERIOD, MODULO_POSITION, FIRST_TRAVEL_SPEED, LAST_TRAVEL_SPEED, ACCELERATION, JERK, and INITIAL Position. Some of these parameters can be changes in an application program using other MLPmp function blocks

A MLPmpRel function block is used to make a bi directional motion. First movement in one direction, then a return motion back to the initial position. A MLPmpAbs function block is use to move one direction to an absolute position.


  • Pmp objects are normally created in the Pipe Network using the graphical engine. Then you do not have to add MLPmpInit function blocks to their programs. Parameters are entered directly in pop-up windows, and the code is then automatically added to the current project.

Arguments

Input

BlockID Description ID Name of a PMP function block in the Pipe Network
  Data type DINT
  Range [-2147483648, 2147483648]
  Unit N/A
  Default
ModuloPosition Description Modulo Position for cyclic motion systems expressed in user logical units (Position Rollover Value)
  Data type LREAL
  Range
  Unit User unit
  Default 360.0
Period Description Sampling period of the generator expressed according to the update cycle (e.g. 2.0 means the sampling is done once every 2 cycles)
  Data type LREAL
  Range
  Unit User unit
  Default 1.0
FirstTravelSpeed Description First Travel Speed of the motion
  Data type LREAL
  Range
  Unit User unit/sec
  Default 100.0
LastTravelSpeed Description Last Travel Speed of the motion
  Data type LREAL
  Range
  Unit User unit/sec
  Default 100.0
Acceleration Description Acceleration of the Pmp block motion
  Data type LREAL
  Range
  Unit User unit/sec2
  Default 1000.0
JerkClosed In physics, jerk is the rate of change of acceleration; more precisely, the derivative of acceleration with respect to time Description Jerk
  Data type LREAL
  Range
  Unit User unit/sec3
  Default 0
InitialPosition Description Initial Position of the Pmp block when the Pipe Network is start up
  Data type LREAL
  Range
  Unit User unit
  Default 0
Modulo Description The available modes are Modulo (True) or No modulo (False)
  Data type BOOL
  Range 0, 1
  Unit N/A
  Default

Output

Default (.Q) Description Returns True if the function block is successfully executingSee Function - General Rules for more information.
  Data type BOOL
  Unit N/A

Related Functions

MLPmpReadAccel

MLPmpReadFstSpd

MLPmpReadInitPos

MLPmpReadJerk

MLPmpReadLstSpd

Example

Structured Text

//Initialize  a PMP Pipe Block named “PMP” to a modulo roll over of 360, motion generator sample period of 1,First Travel Speed of 800.0, Second Travel Speed of 20000.0, Accel of 20000.0,Jerk of 520.0, Initial position of 0.0
MLPmpInit( PipeNetwork.Pmp , 360.0, 1.0, 800.0, 20000.0, 20000.0, 520.0, 0, true ) ;

Ladder Diagram

MLPmpInit: LD example

Function Block Diagram

MLPmpInit: FBD example

Go back to the top of the page[Top]