MLPhaReadPhase

Pipe Network motion icon

 FunctionClosed A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Get the phase value of a phaser block.

Arguments

Input

BlockID

Description

ID Name of a Phaser function block in the Pipe Network

 

Data type

DINT

 

Range

[-2147483648, 2147483648]

 

Unit

N/A

 

Default

Output

Phase

Data type

LREAL

Example

Structured Text

 

PresentPhase := MLPhaReadPhase( PipeNetwork.PhaseAdjust );

 

Ladder Diagram

MLPhaReadPhase: LD example

 

Function Block Diagram

MLPhaReadPhase: FBD example

Go back to the top of the page[Top]