MLSyncStart

Pipe Network motion icon

 FunctionClosed A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Start a synchronization of a synchronizer Pipe Block.

Returns TRUE if the function succeeded.

MLSyncStart

Figure 7-111: MLSyncStart

Arguments

Input

BLockID

Description

Name of the Pipe Network Block

 

Data type

DINT

 

Range

[-2147483648, 2147483648]

 

Unit

n/a

 

Default

Output

Default (.Q)

Description

Function BlockClosed A function block groups an algorithm and a set of private data. It has inputs and outputs. Execute Successfully

See Function - General Rules for more information.
 

Data type

BOOL

 

Unit

n/a

Example

Structured Text

 

MLSyncStart( PipeNetwork.SYN );

 

Ladder Diagram

MLSyncStart: LD example

Function Block Diagram

MLSyncStart: FBD example