MLSyncStop

Pipe Network motion icon

 FunctionClosed A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - De-synchronizes a synchronizer Pipe Block.

Returns TRUE if the function succeeded.

MLSyncStop

Figure 7-112: MLSyncStop

Arguments

Input

Position

Description

Motion Stop Position

 

Data type

LREAL

 

Range

 

Unit

User unit

 

Default

Output

Default (.Q)

Description

Function BlockClosed A function block groups an algorithm and a set of private data. It has inputs and outputs. Execute Successfully

See Function - General Rules for more information.
 

Data type

BOOL

 

Unit

n/a

Example

Structured Text

 

MLSyncStop( PipeNetwork.SYN , 120 );

 

Ladder Diagram

MLSyncStop: LD example

 

Function Block Diagram

MLSyncStop: FBD example