udpSendToVar

PLCopen motion icon

 FunctionClosed A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - sends the contents of a local variable to another controller. This allows for the exchange of data across controllers.

Arguments

Input

En Description Execute the function
  Data type BOOL
  Range [0,1]
  Unit N/A
  Default
sock Description Socket number, return value from udpCreate
  Data type DINT
  Range [0,+65535]
  Unit N/A
  Default
add[] Description Array which contains information about the sender (server) of information. This includes the sender's IP address.
  Data type USINT
  Range [0,32]
  Unit N/A
  Default
varName Description The name of a variable (or array or structure) to send to the receiver. The variable should be the same type as what is expected by the receiver. See udpRcvFromVar.
  Data type  
  Range  
  Unit N/A
  Default

Output

OK Description Returns true when the function successfully executes. See Function - General Rules.
  Data type BOOL
  Unit N/A

Examples

Structured Text

            udpSendToVar( Socket_Number, Add, MyUDPVar )

Ladder Diagram

Function Block Diagram

Go back to the top of the page[Top]